Processor Expert creates incorrect MUX value for Kinetis FlexBus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert creates incorrect MUX value for Kinetis FlexBus

Jump to solution
2,599 Views
leccy
Contributor III

I have tried to implement a FlexBus on CW10.1 with PE for Kinetis K20.

 

The code generated in cpu.c when the RW pin is enabled tried to set MUX[4] for the FB_RW_b pin.  According to the data sheets, this should be MUX[5], along with all the other FlexBus pins.  I cannot find a reference to this in any errata.

 

leccy

0 Kudos
Reply
1 Solution
2,307 Views
ProcessorExpert
Senior Contributor III

Hello,

 

we are sorry for the invonvenience. We will fix it within CW V10.2 update. For now as workaround please add the following row after calling PE_low_level_init:

 

  /* PORTC_PCR11: ISF=0,MUX=5 */
  PORTC_PCR11 = (uint32_t)((PORTC_PCR11 & (uint32_t)~0x01000200UL) | (uint32_t)0x0500UL);

best regards
Vojtech Filip
Processor Expert Support Team

View solution in original post

0 Kudos
Reply
2 Replies
2,308 Views
ProcessorExpert
Senior Contributor III

Hello,

 

we are sorry for the invonvenience. We will fix it within CW V10.2 update. For now as workaround please add the following row after calling PE_low_level_init:

 

  /* PORTC_PCR11: ISF=0,MUX=5 */
  PORTC_PCR11 = (uint32_t)((PORTC_PCR11 & (uint32_t)~0x01000200UL) | (uint32_t)0x0500UL);

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply
2,307 Views
leccy
Contributor III

Thanks for the quick reply.

 

Would you also know why the P&E OSJTAG debugger gives a memory error if i configure the FlexBus in PE, and try to debug the project?

 

leccy

0 Kudos
Reply