Processor Expert compiling errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert compiling errors

1,375 Views
mingzhaoli
Contributor II

Hi guys,

Recently i am trying to use Processor Expert to generate codes for PWM on K70F120.

However, after I generated the codes, some errors occurred after compiling.

Errors:

DescriptionLocationResourcePathType
mingw32-make: *** [Generated_Code/Cpu_c.obj] Error 1bsp_twrk70f120mC/C++ Problem
DescriptionLocationResourcePathType
mingw32-make: *** [Sources/Events_c.obj] Error 1bsp_twrk70f120mC/C++ Problem
DescriptionLocationResourcePathType
mingw32-make: *** Waiting for unfinished jobs....bsp_twrk70f120mC/C++ Problem

my events.c:

void PWM_OnCounterRestart(LDD_TUserData *UserDataPtr)

{

  /* Write your code here ... */

PWM_SetPeriodTicks();

PWM_ResetCounter();

PWM_GetCounterValue();

PWM_SetOffsetTicks();

PWM_GetCaptureValue();

PWM_Init();

}

/*

** ===================================================================

**     Event       :  Cpu_OnLLSWakeUpINT (module Events)

**

**     Component   :  Cpu [MK70FN1M0MJ15]

*/

/*!

**     @brief

**         This event is called when Low Leakage WakeUp interrupt

**         occurs. LLWU flags indicating source of the wakeup can be

**         obtained by calling the [GetLLSWakeUpFlags] method. Flags

**         indicating the external pin wakeup source are automatically

**         cleared after this event is executed. It is responsibility

**         of user to clear flags corresponding to internal modules.

**         This event is automatically enabled when [LLWU interrupt

**         request] is enabled.

*/

/* ===================================================================*/

void Cpu_OnLLSWakeUpINT(void)

{

  /* Write your code here ... */

  Cpu_DisableInt();

}

/* END Events */

#ifdef __cplusplus

}  /* extern "C" */

#endif

0 Kudos
Reply
1 Reply

1,196 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello MingZhao,

To investigate your problem correctly and efficiently, please provide us the follows:

1.    your CW version: Start the IDE and click on Help | About CodeWarrior Development Studio. Send me the version and build id.

2.    upload the entire sample code folder(include .project, .c..) in zip format to me. so that i can test it on my side directly.

3.      error screenshot.

thanks!

BEst Regards,

ZhangJun

0 Kudos
Reply