Processor Expert and Expanded Bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Processor Expert and Expanded Bus

1,530 次查看
dporada
Contributor III

When I set up external ram on the FlexBus using processor expert, processor expert tries to make a copy of the external memory in ram.  If I had this much ram available, I wouldn't need to use the FlexBus.

I always need to go into the ProcessorExpert.lcf and remove the references to ram for my project to run.  Is there a way around this?

Thanks,

Don

0 项奖励
回复
3 回复数

1,341 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

you can disable the generation of the linker file, so you it stays as it is.

See Disable my Code Generation | MCU on Eclipse

I hope this helps.

0 项奖励
回复

1,341 次查看
dporada
Contributor III

I was wondering if there is a setting in Processor Expert so it could generate the linker file, but not try to copy the memory into ram.

0 项奖励
回复

1,341 次查看
Petr_H
NXP Employee
NXP Employee

Please write more deatils on what MCU do you use and how it's connected and configured.

A sample project would be great.

best regards

Petr Hradsky

Processor Expert Support Team

0 项奖励
回复