Processor Expert Driver Update for Kinetis KW2 - not working (missing package)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert Driver Update for Kinetis KW2 - not working (missing package)

1,984件の閲覧回数
rafaelsend
Contributor I

Hi,

This might be a silly question, but I'm having issues updating the Processor Expert in CodeWarrior. I'm using the KW21D256 chip on the TWR-KW2 Tower Board, and I was having problems with generating code. Turns out there's an update package for these chips:

Processor Expert Software – Microcontrollers Driver Suite v10.3

When I try to install it, CW says I'm missing "com.freescale.processorexpert.standalone.feature.group10.3.0". I'm not sure what component exactly this is, nor how to install it. As far as I'm aware, I've installed all the updates for Kinetis, but this might be something else.

Any tips?

Thanks,

Rafael

0 件の賞賛
返信
1 返信

1,391件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hi Rafael,

the MKW2xD Service Pack is targeted for Microcontrollers Driver Suite (specifically for version 10.3) only. Unfortunately, MKW2x family is not supported by CodeWarrior. Please refer to Processor Expert Software - Microcontroller Driver Suite for more information and download link. In case of any problems please let us know.

Best Regards,

Lukas

0 件の賞賛
返信