Problems with Processor Expert 10.3 Eclipse Plugin Installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with Processor Expert 10.3 Eclipse Plugin Installation

ソリューションへジャンプ
3,554件の閲覧回数
matthewbaker
Contributor II

Hi

I have attempted to install the newly released Processor Expert 10.3 Eclipse plugin only to hit the following error:

An error occurred while collecting items to be installed session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=null --> [R]com.freescale.processorexpert.standalone_root 10.3.0, action=). The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.

Has anyone else experienced similar problems installing 10.3 (BTW I am conducting a clean install using Win8 and I have also confirmed under linux that the plugin installation fails with the same missing package dependency)

Kind Regards,

Matthew Baker

1 解決策
2,542件の閲覧回数
matthewbaker
Contributor II

UPDATE: I solved the above issue by first installing com.freescale.eclipse.3.7.updater.custom.updatesite.zip prior to the Processor Expert 10.3 Eclipse plugin installation. I ended up finding a download for com.freescale.eclipse.3.7.updater.custom.updatesite.zip here (https://community.freescale.com/servlet/JiveServlet/download/304336-252686/com.freescale.eclipse.3.7...).

元の投稿で解決策を見る

3 返答(返信)
2,542件の閲覧回数
m4l490n
Contributor V

Hello

Does this also works with eclipse neon?

Regards.

Manuel Malagon

0 件の賞賛
返信
2,542件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Manuel,

no, to my knowledge you cannot install the Processor Expert plugins in Neon (I tried, but it stops with an error).

Erich

2,543件の閲覧回数
matthewbaker
Contributor II

UPDATE: I solved the above issue by first installing com.freescale.eclipse.3.7.updater.custom.updatesite.zip prior to the Processor Expert 10.3 Eclipse plugin installation. I ended up finding a download for com.freescale.eclipse.3.7.updater.custom.updatesite.zip here (https://community.freescale.com/servlet/JiveServlet/download/304336-252686/com.freescale.eclipse.3.7...).