Problems with MK66FX1M0VMD18 support in PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with MK66FX1M0VMD18 support in PE

ソリューションへジャンプ
2,393件の閲覧回数
olavbirkeland
Contributor III

Hi

I am creating a project for MK66FX1M0VMD18 from scratch using KDS 3.0 and PE.

I am running the new project wizard (File -> New -> Kinetis Project ...) and select the processor:

pastedImage_1.png

Then I select KSDK and PE:

pastedImage_2.png

I select Finish and PE genrates code. Then I have to change to the correct processor package, the default is QFP, I am using MAPBGA

Default:

pastedImage_3.png

Is changed to:

pastedImage_4.png

Then the problems starts. PE complains about problems in pin muxing and ask if I want to switch to MK66FN2.... However this is the 2MByte part I am using the 1MByte part!

(In addition and N instead of X in part number, don't remember the meaning of that just now but not correct anyway))

pastedImage_6.png

If I do the switch anyway I end up with the following error, probably becauce I have selected the 1MByte variant, but PE insists on using the 2MByte variant for some tests.

pastedImage_7.png

Can anyone help me?

0 件の賞賛
返信
1 解決策
1,992件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have reproduced the issue and I have also reported the defect to Processor Expert development team.

You can use the following workaround:

When you create a new MK66FX1M0 project, navigate to Component Library and select MK66FX1M0x:

pastedImage_0.png

Select the 144-pins MAPBGA package

pastedImage_1.png

Click on the Finish button. The MK66FX1M0VMD18 CPUs are added and no error is reported (when the configuration is switched in PinSettings).

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,992件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have reproduced the issue and I have also reported the defect to Processor Expert development team.

You can use the following workaround:

When you create a new MK66FX1M0 project, navigate to Component Library and select MK66FX1M0x:

pastedImage_0.png

Select the 144-pins MAPBGA package

pastedImage_1.png

Click on the Finish button. The MK66FX1M0VMD18 CPUs are added and no error is reported (when the configuration is switched in PinSettings).

Best Regards,

Marek Neuzil

0 件の賞賛
返信
1,992件の閲覧回数
olavbirkeland
Contributor III

Hi Marek. I have tried the workaround and it worked. Thanks so mutch

0 件の賞賛
返信