PN7642 code read protect

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7642 code read protect

1,518 Views
KB1
Contributor II

I am using the PN7642 processor and need to protect the user firmware image.

Based on the API, I am using "PN76_Sys_OTPConfigs_EnableCRP()" which is returning 0x07 "PN76_STATUS_AUTH_ERROR" which is NOT one of the expected returns documented in the API.

Can you please provide a detailed example of the process of activating Code Read Protection on this processor?  There is little to no information beyond the actual function call documented in the API.

 

0 Kudos
Reply
0 Replies