PEx generated code directory path change

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PEx generated code directory path change

3,479件の閲覧回数
aymanrjab
Contributor I

Hi,

Please, I would like to know how could I change the generation directory path in processor expert on S32 Design Studio?

Thank you in advance.

0 件の賞賛
返信
3 返答(返信)

3,252件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Click into that field and enter the new name of the folder?

I hope this helps,

Erich

0 件の賞賛
返信

3,252件の閲覧回数
aymanrjab
Contributor I

Hi Erich,

Thank you for your reply.

Unfortunately this doesn't help :smileysad:

1) Changing only the name will create a folder into the current project folder with the new name ProjectFolder->NewFolder

2) I experienced to give a new name with a path like NewFolder/NewSubfolder and it works! ProjectFolder->NewFolder->NewSubfolder

However, if I tried to give a path outside of the project current folder e.g ../../NewFolder this will not work!! and this is blocking for me, because I want to generate the files outside the whole S32DS workspace! and this is why I would like to check with you, if there is any solution to do that?

Thank you in advance

0 件の賞賛
返信

3,252件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I think if you want the files outside the project folder, you have to copy them (e.g. with a script file).

I only have used them inside the project folder for my projects.

Best regards,

Erich

0 件の賞賛
返信