PE fails to generate code if the project path contains parentheses (CW10.2)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE fails to generate code if the project path contains parentheses (CW10.2)

ソリューションへジャンプ
2,356件の閲覧回数
Ainslie
Contributor II

Is this a PE issue or an eclipse issue, as I am porting over from V7.1.

 

ie.  \firmware\(DC00521)\main\ProcessorExpert.pe

 

 

ラベル(1)
タグ(1)
1 解決策
1,781件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

this is a PE issue, it reports:

Description    Resource    Path    Location    Type
ERROR: Project path contains unsupported characters - brackets    test(pe)        Cpu    Processor Expert Problem

Not sure why this is not supported, but I pass this to the engineering team.

 

Normal CodeWarrior/Eclipse projects can have () in the path. I know that there are things like ';' not supported, btw.

 

BK

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,782件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

this is a PE issue, it reports:

Description    Resource    Path    Location    Type
ERROR: Project path contains unsupported characters - brackets    test(pe)        Cpu    Processor Expert Problem

Not sure why this is not supported, but I pass this to the engineering team.

 

Normal CodeWarrior/Eclipse projects can have () in the path. I know that there are things like ';' not supported, btw.

 

BK

0 件の賞賛
返信
1,781件の閲覧回数
Robinwithu
Senior Contributor I

Hello Erich,

I am also getting the same error

(

ERROR: Project path contains unsupported characters - brackets    test(pe)   Cpu    Processor Expert Problem

)

for MC9S08RN8 µC for Codewarrior 10.5, have you got the answer?

BR

Robin

0 件の賞賛
返信
1,781件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Robin,

to my understanding this will not be changed, so you have to remove the (...) from your path. Would that be an issue?

Erich

1,781件の閲覧回数
Robinwithu
Senior Contributor I

Thank you Erich.

Kind Regards

Robin

0 件の賞賛
返信