PE components template error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE components template error

1,441件の閲覧回数
rqbh
Contributor III

Hi , when i turn PE dev mode on, there is one line warning message in console as blow:


:{{DEVELOPMENT}} WARNING: Component GenericSWSPI was stored in the template in newer version: 01.018>01.001

and  stopped in creating shared spi(0%) shown in status bar.

What reason can cause that problem ?

I'm using CW10.5 and PE 10.3.

0 件の賞賛
返信
1 返信

1,221件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Kevin,

the reason is a bug in Processor Expert: it can get stuck while creating a shared component (I already have reported that problem).

To solve the problem, I have changed the setting of the component so the SPI bus is disabled at creation time (so you need to enable it after you have added the component).

Attached is the component with the workaround.

I hope this helps,

Erich

0 件の賞賛
返信