PE components template error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PE components template error

1,498 Views
rqbh
Contributor III

Hi , when i turn PE dev mode on, there is one line warning message in console as blow:


:{{DEVELOPMENT}} WARNING: Component GenericSWSPI was stored in the template in newer version: 01.018>01.001

and  stopped in creating shared spi(0%) shown in status bar.

What reason can cause that problem ?

I'm using CW10.5 and PE 10.3.

0 Kudos
Reply
1 Reply

1,278 Views
BlackNight
NXP Employee
NXP Employee

Hi Kevin,

the reason is a bug in Processor Expert: it can get stuck while creating a shared component (I already have reported that problem).

To solve the problem, I have changed the setting of the component so the SPI bus is disabled at creation time (so you need to enable it after you have added the component).

Attached is the component with the workaround.

I hope this helps,

Erich

0 Kudos
Reply