PE - SPI attribute set list problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE - SPI attribute set list problem

2,874件の閲覧回数
roytrapp
Contributor I

Hello at everyone :smileyhappy:,

i want to transfer data from the MK10DXVLH7 to the DAC7616 per SPI Module.

Can some tell me, what i have to do to solve my problem?

I can't select any entry in the Processor Expert SPI configuration (attribute set list).

Why I can not type in the times, which are given in the datasheet?

Please look at the picture i added.

Thanks for your help,

Roy

0 件の賞賛
返信
1 返信

2,769件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Roy Trapp ,

About your question, I have checked your picture , If you want to choose the data under "Clock rate index"

of Attribute set list, first you need to configure more than one "Clock rate" , in default , there is only one clock

rate setting , so there is no option we can use under it .

Open "Clock rate" configuration view, choose "list of values" in "Runtime settings type", then configre values:

pastedImage_1.png

After do this , you can use the "Clock rate index" list .

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信