PE ADC "High" Level Component Problem for 56F827xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PE ADC "High" Level Component Problem for 56F827xx

709 次查看
dynapb
Contributor IV

Hi All

I am setting up a PE ADC High level component and am having a problem with the Internal Trigger, Trigger Input settings.  This is for a 56F82748 DSC and using the 12 Bit Cyclic ADC.

I get the following error in the setttings.

pastedImage_1.png

and in the Problems it shows the following Errors.

pastedImage_2.png

The strange thing is that the ADC_LDD driver that the ADC High level component uses is happy...

... and it is set to the same TA0_OUT.

pastedImage_5.png

The error message seems to indicate that the XBAR is not set up properly.  So I added it and the "Automatic" settings show that the timer I am using is routed to the ADC.

pastedImage_4.png

To me this seems like a bug but maybe I missed something.

Thanks for your Help!

Pete

标签 (1)
0 项奖励
回复
0 回复数