PCIe NVMe boot in iMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe NVMe boot in iMX8MP

3,507 Views
santhana-kumar
Contributor I

Hi,

We have a custom board based on iMX8MP.

The board currently supports SD and eMMC boot.

Also the board has a provision for M.2 slot, through which we are able to connect WiFi card and works perfectly in kernel side.

Currently, our customer requirement is to enable boot from NVMe SSD.

I checked our u-boot source; I could find PCIe driver support for iMX6 but unable to find support for iMX8MP.

Can you please help to support NVMe SSD based booting in iMX8MP.

Our u-boot is based on https://source.codeaurora.org/external/imx/uboot-imx.git branch imx_v2020.04_5.4.70_2.3.0

If you already have support for NVMe SSD boot in iMX8MP, please provide relevant source code information.

Thanks!

 

Regards,

Santhana Kumar

0 Kudos
Reply
2 Replies

2,653 Views
coindu
Contributor IV

May i ask hhis problem has been resolved?

0 Kudos
Reply

2,996 Views
cosmos
Contributor I

请问您的问题解决了吗

0 Kudos
Reply