My program really exceeded the size of 8kb??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

My program really exceeded the size of 8kb??

953 次查看
williankleber
Contributor I

This is my first program in KDS. I was adding functionalities in Processor Expert, but, after adding the serial communication components, I can no longer add lines of code.

/* ###################################################################
**     Filename    : main.c
**     Project     : teste ADC
**     Processor   : MKE04Z8VFK4
**     Version     : Driver 01.01
**     Compiler    : GNU C Compiler
**     Date/Time   : 2017-03-16, 10:52, # CodeGen: 0
**     Abstract    :
**         Main module.
**         This module contains user's application code.
**     Settings    :
**     Contents    :
**         No public methods
**
** ###################################################################*/
/*!
** @file main.c
** @version 01.01
** @brief
**         Main module.
**         This module contains user's application code.
*/         
/*!
**  @addtogroup main_module main module documentation
**  @{
*/         
/* MODULE main */


/* Including needed modules to compile this module/procedure */
#include "Cpu.h"
#include "Events.h"
#include "AD1.h"
#include "AdcLdd1.h"
#include "TI1.h"
#include "TimerIntLdd1.h"
#include "TU1.h"
#include "LED1.h"
#include "BitIoLdd1.h"
#include "LED2.h"
#include "BitIoLdd2.h"
#include "LED3.h"
#include "BitIoLdd3.h"
#include "LED4.h"
#include "BitIoLdd4.h"
#include "pnCargaCalda.h"
#include "BitIoLdd5.h"
#include "AS1.h"
#include "ASerialLdd1.h"
/* Including shared modules, which are used for whole project */
#include "PE_Types.h"
#include "PE_Error.h"
#include "PE_Const.h"
#include "IO_Map.h"
/* User includes (#include below this line is not maintained by Processor Expert) */

unsigned int nrCountTmr100ms = 0;
byte idMeasure, idGetVal;
bool idReadyADC = FALSE;
word vlAdcAlta[4], vlAdcBaixa[4];
unsigned int nrTempoLed[4] = {0x40,0x40,0x40,0x40};
unsigned int nrContTempoLED[4];
unsigned char nrCountTempNivel[4] = {0x0,0x0,0x0,0x0};
unsigned char idNivelCalda[4] = {0x0,0x0,0x0,0x0};
byte idSendMsg = 0;
bool idTmr1 = FALSE;
bool idLeituraAlta = FALSE; // Indica que a leitura de níveis será feita com 5 V aplicado na calda.

/*lint -save  -e970 Disable MISRA rule (6.3) checking. */
int main(void)
/*lint -restore Enable MISRA rule (6.3) checking. */
{
  /* Write your local variable definition here */
  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
  PE_low_level_init();
  /*** End of Processor Expert internal initialization.                    ***/

  /* Write your code here */
  for(;;){
       if (idTmr1){
            idTmr1 = FALSE;
            if (idNivelCalda[0]){
                 if (++nrContTempoLED[0] >= nrTempoLed[0]){
                      LED1_NegVal();
                      nrContTempoLED[0] = 0;
                 }
            } else {
                 LED1_SetVal();
            }
            if (idNivelCalda[1]){
                 if (++nrContTempoLED[1] >= nrTempoLed[1]){
                      LED2_NegVal();
                      nrContTempoLED[1] = 0;
                 }
            } else {
                 LED2_SetVal();
            }
            if (idNivelCalda[2]){
                 if (++nrContTempoLED[2] >= nrTempoLed[2]){
                      LED3_NegVal();
                      nrContTempoLED[2] = 0;
                 }
            } else {
                 LED3_SetVal();
            }

            if (idNivelCalda[3]){
                 if (++nrContTempoLED[3] >= nrTempoLed[3]){
                      LED4_NegVal();
                      nrContTempoLED[3] = 0;
                 }
            } else {
                 LED4_SetVal();
            }

       }
       if (nrCountTmr100ms >= 100){
            nrCountTmr100ms = 0;
            if (idLeituraAlta){
                 pnCargaCalda_SetVal();
            } else {
                 pnCargaCalda_ClrVal();
            }

            idMeasure = AD1_Measure(FALSE);
       }
       if (idReadyADC){
            if (idLeituraAlta){
                 idGetVal = AD1_GetValue16(vlAdcAlta);
            } else {
                 idGetVal = AD1_GetValue16(vlAdcBaixa);
            }

            idLeituraAlta = !idLeituraAlta;
            idReadyADC = FALSE;
            /*
            for (int i = 0; i <= 3; i++){
                 nrTempoLed[i] = (vlAdcAlta[i] / 20) / 10;
            }
            */
       }

       if (idGetVal == 0x00U){
            for (int i = 0; i <= 3; i++){
                 //AS1_SendChar(0x02);
                 if (vlAdcAlta[i] > vlAdcBaixa[i]+20){
                      if (++nrCountTempNivel[i] >= 20){
                           idNivelCalda[i] = 1;
                           nrCountTempNivel[i] = 10;
                      }
                 } else {
                      if (--nrCountTempNivel[i] <= 0){
                           idNivelCalda[i] = 0;
                           nrCountTempNivel[i] = 10;
                      }
                 }
            }
            idGetVal = 0xFF;
       }
  }

  /*** Don't write any code pass this line, or it will be deleted during code generation. ***/
  /*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
  #ifdef PEX_RTOS_START
    PEX_RTOS_START();                  /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of RTOS startup code.  ***/
  /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
  for(;;){}
  /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/

/* END main */
/*!
** @}
*/
/*
** ###################################################################
**
**     This file was created by Processor Expert 10.5 [05.21]
**     for the Freescale Kinetis series of microcontrollers.
**
** ###################################################################
*/

If I uncomment the line 145 of the code above, I get this error messages:

179705_179705.jpgUntitled-2.jpg

 

This is the image of my PE with the components added. Note that in the console window, the size of program with the line 145 commented.

179689_179689.jpgUntitled-1.jpg

 

My program really this big? Did I do something wrong? that caused this problem?

 

thanks in advance for your time

Original Attachment has been moved to: teste-ADC.zip

标记 (1)
0 项奖励
回复
0 回复数