Multiple PEX files in one project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple PEX files in one project?

Jump to solution
3,353 Views
Daniel_Wax
NXP Employee
NXP Employee

Is it possible (In S32Design Studio for Power) to have multiple  processor expert files in a single project (to support multiple hardware configurations) and then just disable or deselect one that is not targeted for the current board.  In other words only have one enabled at a time.   Of course we would need to regenerate the code each time we switch.

Is this possible?

Labels (2)
0 Kudos
Reply
1 Solution
3,244 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

No, this is not possible.

I see only way to have multiple ProcessorExpert.pe files and change them according to need.

However autosar support this feature.

regards,

Peter

View solution in original post

0 Kudos
Reply
2 Replies
3,244 Views
ErichStyger
Specialist I

Hi Daniel,

I'm using Processor Expert configurations for this, see Configurations with Processor Expert | MCU on Eclipse 

I hope this helps,

Erich

0 Kudos
Reply
3,245 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

No, this is not possible.

I see only way to have multiple ProcessorExpert.pe files and change them according to need.

However autosar support this feature.

regards,

Peter

0 Kudos
Reply