Missing Option new Processor expert project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Missing Option new Processor expert project

2,053 次查看
puzunovic
Contributor I

Hello everybody,

I am new to the NXP s32k family and also new to the s32 design studio.

I have installed latest version and latest update UP9.

I followed few steps form the "Getting started Processor Expert Software –
Microcontrollers Driver Suite
" to create simple new project for s432k144 MCU, but I am missing option

Select File > New > Select File > New > Processor Expert Project from the IDE menu bar.

I cannot create new project using Processor Expert, I cannot add processor expert to the new project. I can create new project from example which contains processor expert, and then it works fine.

PE seemed to be installed, but I am missing option to create new project with PE.

Thanks in advanced

Petar Uzunovic

0 项奖励
回复
2 回复数

1,932 次查看
martin_kovar
NXP Employee
NXP Employee

Hello Petar,

Processor Expert is only tool for creating SDK settings like pin settings and other peripheral settings. This means, your project must contain SDK, then you can work with Processor Expert properly.

The easiest way, how to create SDK based project, is select SDK in startup wizard, please see the figures below.

Select microcontroller you want to use and insert project name. Click Next.

pastedImage_1.png

Click "three dots" button in the SDKs row...new window will apear, then select appropriate SDK. I recommend to use RTM 3.0.0 SDK only. Click OK then click Finish.

pastedImage_2.png

Processor Expert and some other windows will be opened.

pastedImage_3.png

If you have any other question, please feel free to write me back.

Regards,

Martin

1,932 次查看
puzunovic
Contributor I

Hello Martin,

Thank you, this short tutorial helped me and solved my problem.

Kind regards

Petar Uzunovic

0 项奖励
回复