MPC 5775E LED blinking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC 5775E LED blinking

2,147件の閲覧回数
Krishna_Yalamanchili
Contributor I

Hi,

I have taken hello world example from MPC5777C to blink LED on MPC5775E.Unfortunately LED is not blinking. What am I doing wrong?

0 件の賞賛
返信
2 返答(返信)

1,886件の閲覧回数
RachelGomez123
Contributor I

Another thing that commonly causes flickering in LED bulbs is loose connections or circuits. This is easy to fix. Just screw the LED bulb in tighter to see of that fixes the problem. If there's a lot of dust in the fixture, first blow out the connection points to remove the dust before putting the bulb back in.

 

Regards,

Rachel Gomez

0 件の賞賛
返信

2,127件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached is working project for MPC5775E-EVB (S32DS 2.1 and SDK RTM 3.0.3). You just need to use wire to connect pin PTF[20] to LED. So, connect pin 2 of J125 header to some LED on JP6 header.

lukaszadrapa_0-1656070383095.pnglukaszadrapa_0-1656070383095.png

Hope it helps.

Regards,

Lukas

0 件の賞賛
返信