MPC 5510 Interrupt Disable and Enable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC 5510 Interrupt Disable and Enable

2,591件の閲覧回数
pederrogo
Contributor III

Hello,

 

Turning off and on all interrupts is typically done by:

asm(" wrteei 0");

asm (" wrteei 1");

 

But, how to just disable a certain interrupt or group of interrupts?

Or is it possibly to just disable interrupts configured with a prio below a certai level?

 

Best Regards,

 

Peder Rogö

 

 

Peder Rogö

Senior SW Design Engineer

 

CPAC SYSTEMS AB

Box 217

SE-401 23 Göteborg

Visitors: Bergskroken 3, Mölndal

Phone: +46 (0)31 352 16 00

Mobile: +46 (0)707 218740

[email protected]

http://www.cpacsystems.se

 

TAKING CONTROL FORWARD

 

This email message (including its attachments) is confidential and may contain privileged information and is intended solely for the use of the individual and/or entity to whom it is addressed. If you are not the intended recipient of this e-mail you may not disseminate, distribute or copy this e-mail (including its attachments), or any part thereof. If this e-mail is received in error, please notify the sender immediately by return e-mail and make sure that this e-mail (including its attachments), and all copies thereof, are immediately deleted from your system. Please further note that when you communicate with us via email or visit our website we process your personal data. See our privacy policy for more information about how we process it: https://www.volvogroup.com/en-en/privacy.html

 

0 件の賞賛
返信
2 返答(返信)

2,560件の閲覧回数
pederrogo
Contributor III

Hi Lukas,

Thanks for your support. We will look into to this in the quite near future and come to you if we would need any further support.

Regards,

Peder

0 件の賞賛
返信

2,574件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

an interrupt can be enabled/disabled on three levels:

- MSR[EE] bit

- priority level

- local interrupt enable bit in a peripheral (like PITINTEN register, for example)

If all three conditions are satisfied, an interrupt will be triggered. If an interrupt is disabled on one or on more levels, it won't be triggered.

MSR[EE] bit and local interrupt enable bits are clear, I think. Regarding the priority, please take a look at section "9.5.5 Priority Ceiling Protocol" in the reference manual. This allows you to disable group of interrupts based on their priority level.

Regards,

Lukas

 

0 件の賞賛
返信