MK20DX256VLK10 vs USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20DX256VLK10 vs USB

1,399件の閲覧回数
mikhailburakov
Contributor III

Hello!

I have issues with USB on a custom board with mk20dx256vlk10 MCU. For some time we used mk20dx256vlk7 (72MHz) chip and everything was working fine.

Later we switched to 100MHz chip. All the modules work without any issues except the USB_LDD. The symptoms are the following:

1) Connect the device to host PC

2) Receive BusSpeedDetect event

3) Never receive DeviceSetupPacket event

4) Host notices connection but can't recognize device (i.e. empty device and vendor id, etc.)

5) Disconnect device from host PC

6) Receive BusSpeedDetect event

This was tested with 2 vkl7 boards and 3 vlk10 boards using different cables and PCs.

I also tested different clock configurations without any success on mk20dx256vlk10.

I checked the references and did not find any differences in USB sections.

Also I created an empty project based on mk20dn512vlk10 PE configuration with only USB_LDD module. The results was the same - USB working on vlk7 and not working on vlk10.

Is there some important configuration I missed? Are there any hardware differences in USB modules? Is this known issue?

P.S. I use CW 10.6.

0 件の賞賛
返信
1 返信

1,223件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

Could you send us your application for further anaylysis of the problem, please? We will try to reproduce the problem and fix it.

Best Regards,

Marek Neuzil

0 件の賞賛
返信