MFG Tool error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFG Tool error

1,630件の閲覧回数
jerry2004
Contributor I

mx6s hardware has been upgraded to a new version. Mfg tool is used to burn and write errors. The errors are as follows:

Write() Error writing to device 0x79.
Failed to initialize memory!

スポイラ
スポイラ
 

But the main chip and DDR remain unchanged。It is felt from log that the uboot in RAM did not run successfully。The same mfg tool can be burned on the old version。I want to know why

I've also calibrated DDR with NXP DDR test tools,Fixed some parameters, it was passed,But the same mistake was reported。

In addition, why in MFG burning process, I have no information output in serial port, how to set it in uboot to output information

0 件の賞賛
返信
1 返信

1,614件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

 

for that error one can check external devices, like emmc,sd or nand, uart serial port.

For example one can test them with jtag and baremetal sdk, "1.1.0_iMX6_Platform_SDK.zip"  from

https://community.nxp.com/t5/i-MX-Processors/SMP-Enable-in-IMX6/m-p/542111

 

Best regards
igor

0 件の賞賛
返信