MFG Tool Linux version is not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MFG Tool Linux version is not working

1,320 次查看
greivin_fallas
Contributor II

Hello all, i tested MFG Tool in Ubuntu 16.04 with i.MX8MQuad Evaluation Kit (using the provided scripts) but i could not load an image because of error code #24. The log message shows 'Invalid device name MX8QM' but according to 'ucl2.xml' (PID, VID and 'lsusb' command) i should get the configuration for MX8MQ.

'ucl2.xml' configuration tags:

<CFG>

<STATE name="BootStrap" dev="MX8QM" vid="1FC9" pid="0129"/>

<STATE name="BootStrap" dev="MX8QXP" vid="1FC9" pid="012F"/>

<STATE name="BootStrap" dev="MX8MQ" vid="1FC9" pid="012B"/>

<STATE name="Updater" dev="MSC" vid="066F" pid="37FF"/>

</CFG> 

I also changed the 'cfg.ini' file but i got the same error.

The same files worked without problems in Windows 8.

What is wrong?

Am i missing something in Linux?

标记 (3)
0 项奖励
回复
0 回复数