MC68336

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC68336

1,803 Views
Bartek0x00
Contributor I

Hi, i have a binary file that runs on MC68336 which i need to disassemble. Most of the tools that work for MC68K dont recognize MC68336 code. Can i get some recommendation to what tools use for MC68336, or what are the differences between this two CPUs?

0 Kudos
Reply
1 Reply

1,776 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bartek0x00 

The MC68336 is part of the Motorola 68300 family of microcontrollers, which are derived from the Motorola 68000 series but include additional features and peripherals tailored for embedded applications. While the core of the MC68336 is based on the 68000 architecture, there are differences in integrated peripherals and some additional instructions specific to the 68300 family.

The current version for 68k is the CodeWarrior for 68k V3.2.

Extract of the Developer Notes - E68K-CF Tools.txt file

Hope this will help you.

BR

Hang

0 Kudos
Reply