LWIP with Processorexpert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LWIP with Processorexpert

1,724 Views
serhatitu
Contributor III

Has anyone used LWIP with Processorexpert?  I have attached an example, but  it uses SPI for LWIP, may be helpful.

 

Best regards

Original Attachment has been moved to: plc-stamp_1_examples-0.2-beta.zip

Tags (2)
0 Kudos
Reply
1 Reply

1,263 Views
Petr_H
NXP Employee
NXP Employee

Hi,

Thanks for the example. Unfortunatelly there are currently no plans for including support for LWIP into Processor Expert as a component.

However, it could be possible to add to application, like you did, and use Processor Expert Ethernet  component.

Best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply