[LS1028A]:How to access devices,which are connected through I2C HUB ?.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[LS1028A]:How to access devices,which are connected through I2C HUB ?.

跳至解决方案
11,396 次查看
Amit_Keshri
Contributor III

Dear NXP Team,

In our LS1028A based custom board 5 different devices are connected through I2C hub (TCA9548APWR) in bus-2 as shown in attached file.

I am able to read and write in i2c devices connected through I2C Hub in U-Boot but same thing is not happening in Linux when i am trying to write and read through  i2ctransfer utility and separate application and getting Resource temporarily unavailable(using own app).

In U-Boot 1st i am writing in i2c hub to select devices connected to hub then i am writing in devices and getting correct data as shown below:

-----------------------
#TO check RTC:
i2c probe
i2c dev 2
i2c probe
i2c mw 0x71 0x0 0x1   (0x71 is I2C Hub address)
i2c probe
i2c mw 0x51 0xa2 0xe (0x51 in RTC address
i2c md 0x51 0xa2 0x1
------------------------
#TO check EEPROM2:
i2c mw 0x71 0x0 0x2
i2c probe
i2c mw 0x50 0x0 0xf
i2c md 0x50 0x0 0x1

 

But in linux with below i am using below utility:

i2ctransfer 2 w17@0x71 0x0 0xff-      (to write  0xff in i2c hub address 0x71 to enable all i2c hub                                                                                                                                                   devices)

2ctransfer 2 w1@0x71 0x0 r1              (to read in i2c hub address 0x71)

i2ctransfer 2 w17@0x51 0x0 0x77-    (to write  0x77 in RTC devices of hub address 0x51 )                                                                                                          

2ctransfer 2 w1@0x51 0x0 r1             (to read  RTC hub address 0x51)

But not getting proper data with utility.

I have attached required file with this post.

Below are my question:

With i2ctransfer utility i am able to read and write other EEPROM(@0x50) devices but why i could not able to read and write the devices which are connected through i2c hub,even after enabling i2c devices by writing in i2c hub?.

What changes are required in dts and .config file to access i2c hub devices ?.

Please help me on this.

Thanks & Regards,

Amit Keshri

 

0 项奖励
回复
1 解答
10,215 次查看
Amit_Keshri
Contributor III

Hi @yipingwang ,

I2C Hub devices is working in linux and we are able to read and write without any hardware change and below are the changes in Software:

I2C Hub dts changes:

&i2c1 {
status = "okay";
/* i2c-sda-hold-time-ns = <1000>; */
/* clock-frequency = <0x186a0>; */

i2c-mux@71 {
/*compatible = "ti,tca9548"; */
compatible = "nxp,pca9548";
/* compatible = "ti,tca9539"; */
#address-cells = <1>;
#size-cells = <0>;
reg = <0x71>;

i2c@1 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x1>;

rtc_dev@51 {
#sound-dai-cells = <0>;
compatible = "nxp,pcf2129";
reg = <0x51>;
};
};

i2c@2 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x02>;

eeprom@50 {
compatible = "nxp,pca9847";
/*compatible = "nxp,24lc02"; */
reg = <0x50>;
#shunt-resistor = <500>;
};
};

i2c@3 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x3>;

pcie@38 {
compatible = "nxp,sa56004";
reg = <0x38>;
#vcc-supply = <&sb_3v3>;
};

};
i2c@4 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x4>;

temp-sensor@4d {
compatible = "nxp,sa56004";
reg = <0x4d>;
#vcc-supply = <&sb_3v3>;
};

};

i2c@5 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x5>;

xmc_conn:xmc@4d {
compatible = "nxp,sa56004";
reg = <0xd>;
#vcc-supply = <&sb_3v3>;
};

};
};
};

To Access I2C devices which are connected through I2C HUB:we are opening below device files name for read and write in our application:

for I2C HUB: "/dev/i2c-1"

RTC: "/dev/i2c-2"

EEPROM: "/dev/i2c-3

PCIe: "/dev/i2c-4"

Temperature sensor: "/dev/i2c-5"

we are writting 0xff to 0x0 register to I2C Hub(0x71) before to access above i2c hub devices.

Regards,

Amit Keshri

 

在原帖中查看解决方案

0 项奖励
回复
9 回复数
11,367 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following i2c switch example in Documentation/devicetree/bindings/i2c/i2c-mux-pca954x.txt.

Example:

i2c-switch@74 {
compatible = "nxp,pca9548";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x74>;

interrupt-parent = <&ipic>;
interrupts = <17 IRQ_TYPE_LEVEL_LOW>;
interrupt-controller;
#interrupt-cells = <2>;

i2c@2 {
#address-cells = <1>;
#size-cells = <0>;
reg = <2>;

eeprom@54 {
compatible = "atmel,24c08";
reg = <0x54>;
};
};

i2c@4 {
#address-cells = <1>;
#size-cells = <0>;
reg = <4>;

 rtc@51 {
compatible = "nxp,pcf8563";
reg = <0x51>;
};
};
};

Please refer to PCA954x I2C mux/switch driver in drivers/i2c/muxes/i2c-mux-pca954x.c.

0 项奖励
回复
11,361 次查看
Amit_Keshri
Contributor III

Dear NXP Support Team,

Thank you for your reply.

I will check and update You.

 

Regards,

Amit Keshri

0 项奖励
回复
11,358 次查看
Amit_Keshri
Contributor III

Dear NXP support Team,

I refer the dts file for i2c hub in  Documentation/devicetree/bindings/i2c/i2c-mux-pca954x.txt and i also check  Documentation/devicetree/bindings/i2c/i2c-mux.txt folder and modified my dts file but still i couldn't able to access i2c hub device((TCA9548APWR) and when i am trying to write any data from i2c hub devices through it is showing  error as shown below:

root@TinyLinux:/usr/sbin# i2ctransfer 1 w17@0x71 0x0 0xff-
i2ctransfer: WARNING! This program can confuse your I2C bus
Continue? [y/N] y
i2ctransfer: I2C_RDWR: Resource temporarily unavailable

Below is my dts file for i2c_hub :

&i2c2 {
status = "okay";
i2c-sda-hold-time-ns = <1000>;
clock-frequency = <0x186a0>;

i2c-mux@71 {
compatible = "nxp,pca9548";
reg = <0x71>;
#address-cells = <1>;
#size-cells = <0>;

i2c@1 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x1>;

rtc:rtc_dev@51 {
#sound-dai-cells = <0>;
compatible = "nxp,pcf2129";
reg = <0x51>;
};
};

i2c@2 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x02>;

eeprom:eeprom@50 {
compatible = "nxp,24lc02";
reg = <0x50>;
#shunt-resistor = <500>;
};
};

i2c@4 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x4>;

temp_sensor:temp-sensor@4d {
compatible = "nxp,sa56004";
reg = <0x4d>;
#vcc-supply = <&sb_3v3>;
};

};

};

};

Please tell me where i am doing wrong ?.

What further modification is required ?.

Regards,

Amit Keshri

0 项奖励
回复
11,341 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You need to follow drivers/i2c/muxes/i2c-mux-pca954x.c.to create i2c hub device driver for TCA9548APWR device. Then update "compatible" property in i2c-mux@71 device node.

0 项奖励
回复
11,260 次查看
Amit_Keshri
Contributor III

Hi yipingwang,

Thank you for your reply.

followed drivers/i2c/muxes/i2c-mux-pca954x.c and created i2c hub device driver for TCA9548APWR device as attached with this post.

Below is my dts modifuication:

&i2c2 {
status = "okay";
// i2c-sda-hold-time-ns = <1000>;
// clock-frequency = <0x186a0>;

i2c-mux@71 {
compatible = "ti,tca9548";
//compatible = "nxp,pca9548";

#address-cells = <1>;
#size-cells = <0>;
reg = <0x71>;

i2c@1 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x1>;

rtc:rtc_dev@51 {
#sound-dai-cells = <0>;
compatible = "nxp,pcf2129";
reg = <0x51>;
};
};

i2c@2 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x02>;

eeprom:eeprom@50 {
compatible = "nxp,24lc02";
reg = <0x50>;
#shunt-resistor = <500>;
};
};

i2c@3 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x3>;

pcie:pcie@38 {
compatible = "nxp,sa56004";
reg = <0x38>;
#vcc-supply = <&sb_3v3>;
};

};

i2c@4 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x4>;

temp_sensor:temp-sensor@4d {
compatible = "nxp,sa56004";
reg = <0x4d>;
#vcc-supply = <&sb_3v3>;
};

};
};
};

while booting linux it is showing error as given below

 i2c /dev entries driver

tca954x 2-0071: probe failed

I tried to read and write in i2c hub switch as given below:

i2ctransfer 2 w17@0x71 0x4 0x56-
i2ctransfer 2 w1@0x71 0x4 r1

but it is showing "i2ctransfer: I2C_RDWR: Resource temporarily unavailable".

I have attached  for linux booting log file,tca9548 driver code .

Please suggest me what wrong i am doing ?.

Is my dts and driver file for TCA9548 i2c hub switch is correct?.

Regards,

Amit Keshri

0 项奖励
回复
11,250 次查看
yipingwang
NXP TechSupport
NXP TechSupport

In your driver code i2c-mux-tca954x.c, please do the following modification.

{ .compatible = "ti,tca9548", .data = &chips[tca_9548] },

Modify to 

{ .compatible = "ti,tca9548", .data = &chips[tca9548] },

0 项奖励
回复
11,243 次查看
Amit_Keshri
Contributor III

Hi @yipingwang 

Thank You for your reply.

As you suggestion i have added { .compatible = "ti,tca9548", .data = &chips[tca9548] }, in  drivers/i2c/muxes/i2c-mux-tca954x.c file and generated kernel image but it is showing below error while booting kernel:

[ 6.081838] i2c /dev entries driver
[ 6.086363] i2c_set_clientdata, data->client:0x5a071400
[ 6.091801] ret value of i2c_smbus_write_byte:-11
[ 6.096523] ret value of tca954x_init():-11
[ 6.100723] tca954x 1-0071: probe failed
[ 6.104696] i2c_set_clientdata, data->client:0x5a071000
[ 6.110126] ret value of i2c_smbus_write_byte:-11
[ 6.114845] ret value of tca954x_init():-11
[ 6.119041] tca954x 2-0071: probe failed

Note:

Except tca954x 2-0071: probe failed I have  added other print in tca954x.c for debugging.

Please check attached tca954x.c file and booting log file.

What i can do to solve this error?

Please suggest

Regards,

Amit  Keshri

0 项奖励
回复
11,115 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please contact TI to require Linux driver for TCA9548APWR device.

0 项奖励
回复
10,216 次查看
Amit_Keshri
Contributor III

Hi @yipingwang ,

I2C Hub devices is working in linux and we are able to read and write without any hardware change and below are the changes in Software:

I2C Hub dts changes:

&i2c1 {
status = "okay";
/* i2c-sda-hold-time-ns = <1000>; */
/* clock-frequency = <0x186a0>; */

i2c-mux@71 {
/*compatible = "ti,tca9548"; */
compatible = "nxp,pca9548";
/* compatible = "ti,tca9539"; */
#address-cells = <1>;
#size-cells = <0>;
reg = <0x71>;

i2c@1 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x1>;

rtc_dev@51 {
#sound-dai-cells = <0>;
compatible = "nxp,pcf2129";
reg = <0x51>;
};
};

i2c@2 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x02>;

eeprom@50 {
compatible = "nxp,pca9847";
/*compatible = "nxp,24lc02"; */
reg = <0x50>;
#shunt-resistor = <500>;
};
};

i2c@3 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x3>;

pcie@38 {
compatible = "nxp,sa56004";
reg = <0x38>;
#vcc-supply = <&sb_3v3>;
};

};
i2c@4 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x4>;

temp-sensor@4d {
compatible = "nxp,sa56004";
reg = <0x4d>;
#vcc-supply = <&sb_3v3>;
};

};

i2c@5 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0x5>;

xmc_conn:xmc@4d {
compatible = "nxp,sa56004";
reg = <0xd>;
#vcc-supply = <&sb_3v3>;
};

};
};
};

To Access I2C devices which are connected through I2C HUB:we are opening below device files name for read and write in our application:

for I2C HUB: "/dev/i2c-1"

RTC: "/dev/i2c-2"

EEPROM: "/dev/i2c-3

PCIe: "/dev/i2c-4"

Temperature sensor: "/dev/i2c-5"

we are writting 0xff to 0x0 register to I2C Hub(0x71) before to access above i2c hub devices.

Regards,

Amit Keshri

 

0 项奖励
回复