LPC552x SYSTEMRESET vs SWRRWSET

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC552x SYSTEMRESET vs SWRRWSET

ソリューションへジャンプ
4,081件の閲覧回数
_Ferrari_
Contributor V

Dear all,

I noticed that in the register AOREG1 (please refer to UM11126  document) there are two bits:

BIT 7: SYSTEMRESET(the last chip reset was caused by a System Reset requested by the ARM CPU)

and

BIT 9: SWRRESET (The last chip reset was caused by a Software event)

_Ferrari__0-1706728474182.png

 

I'm able to reset the CPU by calling the __NVIC_SystemReset() function but I can't find any routine or any trick to generate a 'software reset event' in order to set the the bit 9 in AOREG1 register.

Did you have a similar problem ?

How did you fix it ?

Thank you very much for your help and cooperation

0 件の賞賛
返信
1 解決策
4,021件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @_Ferrari_ 

       Please do not use Debug. When you run debug and click Stop, the chip will not be detected because the chip keeps resetting.

      You can use the GUI flash tool to download the code and view the reset status on the serial port.

2024-02-04_9-28-49.jpg

Best regards, Alex

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,048件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @_Ferrari_ 

       If you want SWRRESET to position 1, you can do so with the following code:

    PMC->RESETCTRL|=1<<3;
    SYSCON->SWR_RESET= 0x5a000001;

       In my opinion, the __NVIC_SystemReset() function does achieve a reset, but it is actually an operation done to the kernel, not a real software reset.

      I demonstrated with LPC55S69, checking the status of SWRRESET and SYSTEMRESET. Refer to the following figure:

Alex_Wang_0-1706866466174.jpeg

The test code is as follows:

#include "fsl_device_registers.h"
#include "fsl_debug_console.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_power.h"

int main(void)
{
    char ch;

    /* Init board hardware. */
    /* set BOD VBAT level to 1.65V */
    POWER_SetBodVbatLevel(kPOWER_BodVbatLevel1650mv, kPOWER_BodHystLevel50mv, false);
    /* attach main clock divide to FLEXCOMM0 (debug console) */
    CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);

    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitDebugConsole();
#if !defined(DONT_ENABLE_FLASH_PREFETCH)
    /* enable flash prefetch for better performance */
    SYSCON->FMCCR |= SYSCON_FMCCR_PREFEN_MASK;
#endif

    PRINTF("hello world.\r\n");
    if(((PMC->AOREG1>>7)&1)==1)
    {
   	 PRINTF("sysreset=1\r\n");
    }
	 else if(((PMC->AOREG1>>7)&1)==0)
	{PRINTF("sysreset=0\r\n");}


    if(((PMC->AOREG1>>9)&1)==1)
    {
   	 PRINTF("softreset=1\r\n");
    }
	 else if(((PMC->AOREG1>>9)&1)==0)
	{PRINTF("softreset=0\r\n");}

    PMC->RESETCTRL|=1<<3;
    SYSCON->SWR_RESET= 0x5a000001;

	//__NVIC_SystemReset();
    while (1)
    {
        ch = GETCHAR();
        PUTCHAR(ch);
    }
}

Best regards, Alex

 

0 件の賞賛
返信
4,038件の閲覧回数
_Ferrari_
Contributor V

dear @Alex_Wang 

Thank you for your answer.

I just I copied and pasted your software in my 'hello world' sdk example.

I'm using LPC55S28-EVK evaluation board

 

_Ferrari__0-1706872448703.png

 

0 件の賞賛
返信
4,022件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @_Ferrari_ 

       Please do not use Debug. When you run debug and click Stop, the chip will not be detected because the chip keeps resetting.

      You can use the GUI flash tool to download the code and view the reset status on the serial port.

2024-02-04_9-28-49.jpg

Best regards, Alex

0 件の賞賛
返信