K60 UART Interrupt with Processor Expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 UART Interrupt with Processor Expert

2,655件の閲覧回数
tugasakhirroket
Contributor I

Hi everyone!

Now I'm using Code Warrior (with Processor Expert Integration), I want to generate serial communication between Kinetis K60D100M Board and my computer, so far I've successfully send data to my computer via UART3. How can I use UART interrupt mode to receive data from my computer?

Note : I'm using PE wizard to generate the code.

Can anyone help to solve the problem ? Thank you .

タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,873件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

could you please try to check examples on "Typical Usage" page in Component´s help? It is available when you right click on component under Help menu command.

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信

1,873件の閲覧回数
dkarthik
Contributor II

Hi, I'm using TWR K60D100M kit. I tried the "Typical Usage" for both interrupt and Polling mode. Polling mode works for UART5 (USB OSJTAG debugger port) but interrupt mode doesn't work. I enabled NMIT interrupt in Processor and enabled Interrupts in the AS1:serial_LDD component of Processor Expert. Do I have to include something in the typical usage code for interrupt mode of UART or I haven't enabled other interrupts? Pls help

0 件の賞賛
返信