Issue with I2C component and 568000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with I2C component and 568000

Jump to solution
1,857 Views
ivekengineer
Contributor III

Component: InternalI2C

CodeWarrior for MCU 10.3 with updates installed.

Processor: MC56F8257

When I enable this component in my project, I get the following 3 errors:

ERROR: at line 66: Property not found: "CPU_peripheral" (file: Beans\InternalI2C\InternalI2C_56800.chg) MotorMCU  I2C2 Processor Expert Problem

ERROR: Error in the component setting. More details provided by Component Inspector for this component MotorMCU  I2C2 Processor Expert Problem

ERROR: This component is not supported for this CPU yet. MotorMCU  I2C2 Processor Expert Problem

I have had this component in my project for quite a while, but have had it disabled.  I don't remember these errors when I first added it (CodeWarrior 10.3 without updates), so I am wondering whether this is a bug that came along with the most recent updates to 10.3?

Is there something I can do to fix this so I don't have to wait for a new release (i.e., I really want to use this component now).

Thanks!

Tags (3)
0 Kudos
Reply
1 Solution
1,734 Views
Petr_H
NXP Employee
NXP Employee

Hi,

We apologize for an inconvenience. It's a bug that has been already fixed into the latest release. Please download the CW for Microcontrollers V10.4 from the Freescale website http://www.freescale.com/codewarrior/downloads .

best regards

Petr Hradsky

Processor Expert Support Team

View solution in original post

0 Kudos
Reply
1 Reply
1,735 Views
Petr_H
NXP Employee
NXP Employee

Hi,

We apologize for an inconvenience. It's a bug that has been already fixed into the latest release. Please download the CW for Microcontrollers V10.4 from the Freescale website http://www.freescale.com/codewarrior/downloads .

best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply