Is code generated by PE for Kinetis microcontrollers MISRA compliant?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is code generated by PE for Kinetis microcontrollers MISRA compliant?

Jump to solution
2,100 Views
jvasil
Contributor III

We see lots of MISRA violations when looking at drivers produced for the MK64 microcontroller.  Our initial assumption was that this code was not meant to be compliant (with MISRA C 2004) but I recently saw that there were a fair number of postings related to MISRA and started wondering if I was missing something.

If it is supposed to be compliant, is there any sort of compliance statement available?

Thanks,

James

0 Kudos
Reply
1 Solution
1,866 Views
Petr_H
NXP Employee
NXP Employee

Hi,

Currently the drivers are not fully Misra compliant. However we aim to make it compliant (as much possible) in the future. We are moving forward, but it there is currently no date when the goal is planned to be reached.

Best regards

Petr Hradsky

View solution in original post

0 Kudos
Reply
2 Replies
1,866 Views
Petr_H
NXP Employee
NXP Employee

Hi,

Currently the drivers are not fully Misra compliant. However we aim to make it compliant (as much possible) in the future. We are moving forward, but it there is currently no date when the goal is planned to be reached.

Best regards

Petr Hradsky

0 Kudos
Reply
1,866 Views
jvasil
Contributor III

Thanks!

0 Kudos
Reply