Last year I raised a question about having InterruptVector components in PE.
I had a problem with using the RTC component for Kinetis, and needed to use my own code in a PE project, but was unable to add my own interrupt vector.
I was told that the component would be added in 10.3.
other users have also been told the same thing.
已解决! 转到解答。
Hello,
Interruptvector component should be supported from CW V10.4. However from some reason it is not visible when the filter button is on. To show it in Component Library is necessary to switch this button to off. Details attached. We will try to improve this behaviour for next release.
Best regards
Vojtech Filip
Processor Expert Support Team
Thanks Erich
ExtInt only appears to be for a signal on an IO pin.
I want to be able to create my own interrupt vector for an existing vector in the table, in this case for the Kinetis RTC.
I can't do this on a PE project, since PE re-creates the vector table at compile time.
Hello,
Interruptvector component should be supported from CW V10.4. However from some reason it is not visible when the filter button is on. To show it in Component Library is necessary to switch this button to off. Details attached. We will try to improve this behaviour for next release.
Best regards
Vojtech Filip
Processor Expert Support Team
 
					
				
		
 BlackNight
		
			BlackNight
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		That 'filter bug' is still present in MCU10.5, see Processor Expert Component not Showing Up? | MCU on Eclipse
Will it be fixed in 10.6 or in an update?
I see that the filter bug is not only for the InterruptVector component but as well for others? Is there a list of all components affected?
Thanks!