InterruptVector component still not available in CW10.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

InterruptVector component still not available in CW10.3

ソリューションへジャンプ
2,748件の閲覧回数
leccy
Contributor III

Last year I raised a question about having InterruptVector components in PE.

I had a problem with using the RTC component for Kinetis, and needed to use my own code in a PE project, but was unable to add my own interrupt vector.

I was told that the component would be added in 10.3.

other users have also been told the same thing.

0 件の賞賛
返信
1 解決策
2,567件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

Interruptvector component should be supported from CW V10.4. However from some reason it is not visible when the filter button is on. To show it in Component Library is necessary to switch this button to off. Details attached. We will try to improve this behaviour for next release.

Best regards

Vojtech Filip

Processor Expert Support Team

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,567件の閲覧回数
leccy
Contributor III

Filip

Your suggestion also works on 10.3.

Many thanks for the reply


0 件の賞賛
返信
2,567件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

yes, have a look at the 'ExtInt' component. I'm using MCU10.4, but I believe it had been added already in 10.3

0 件の賞賛
返信
2,567件の閲覧回数
leccy
Contributor III

Thanks Erich

ExtInt only appears to be for a signal on an IO pin.

I want to be able to create my own interrupt vector for an existing vector in the table, in this case for the Kinetis RTC.

I can't do this on a PE project, since PE re-creates the vector table at compile time.

0 件の賞賛
返信
2,568件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

Interruptvector component should be supported from CW V10.4. However from some reason it is not visible when the filter button is on. To show it in Component Library is necessary to switch this button to off. Details attached. We will try to improve this behaviour for next release.

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信
2,567件の閲覧回数
BlackNight
NXP Employee
NXP Employee

That 'filter bug' is still present in MCU10.5, see Processor Expert Component not Showing Up? | MCU on Eclipse

Will it be fixed in 10.6 or in an update?

I see that the filter bug is not only for the InterruptVector component but as well for others? Is there a list of all components affected?

Thanks!

0 件の賞賛
返信
2,567件の閲覧回数
leccy
Contributor III

Many thanks Filip.

I will download 10.4 and give it a go.

0 件の賞賛
返信