IO_map.h

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IO_map.h

1,491 Views
norbertoj
Contributor III


I have problems with Process Expert, I generated the auto code of my Processor MK60DN512VLQ10 and it did IO_map.h with target to MK60D10.h (Static_Code), the problem is that the builder are taking two mappings, the file MK60D10.h (Static_Code) and the MK60DZ10.h of Processor Expert and TWRK60DN512, I can't change the paths of the builder because I get error of compilation in psp directory. I don't know why it's taking two mapping files.

0 Kudos
Reply
1 Reply

1,318 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto,

Please take a screenshot about the steps when you create the project ,

then we can reproduce the problem . Also tell me the IDE version.

BR

Alice

0 Kudos
Reply