IMX8mm rtnet Oops

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8mm rtnet Oops

3,995件の閲覧回数
robyli
Contributor I

HI,xiaodong:

       I'm having trouble trying IMX8mm. linux-imx 5.7.40.2.3.3 from NXP github.and I patch to linux-imx 5.7.40.2.3.3 with  xenomai3.1  I use IMX8mmEVM board.Port rt_fec driver. when  I run rtnet,I'm having the following problem。

 

robyli_2-1650250068339.pngrobyli_2-1650250068339.png

robyli_3-1650250093312.pngrobyli_3-1650250093312.png

robyli_4-1650250114957.pngrobyli_4-1650250114957.png

 

 

and  I objdupm  identified some problems。

robyli_5-1650250213001.pngrobyli_5-1650250213001.png

 

I use the resources you posted and run into the same problems. I put in the drivers and patches you released, and I had the same problem。Expect to hear from you。

@xiaodong_zhang 

 

 

 

 

0 件の賞賛
返信
4 返答(返信)

3,904件の閲覧回数
xiaodong_zhang
NXP Employee
NXP Employee

Customer already fix the issue.

0 件の賞賛
返信

3,989件の閲覧回数
xiaodong_zhang
NXP Employee
NXP Employee

Hi Roby,

   i.MX8MM EVK board use AR8031 as Ethernet PHY, but I see it's KSZ9031 in your log. So you don't use iMX official EVK board, right? if yes, you need to check your device tree. In addition, you need to check enable-Xenomai-driver.config in release package of xenomai-arm64, if you apply the config for you kernel config.

0 件の賞賛
返信

3,986件の閲覧回数
robyli
Contributor I

Hi,xiaodong

     yes,I use chunaglong(创龙) IAMX8mm EVM, PHY is KSZ9031,but,PHY   is  attached ,I'll check the configuration again,Thank you。

0 件の賞賛
返信

3,946件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

if chunaglong(创龙) board, I suggest you contacting chunaglong(创龙) for technical support.

0 件の賞賛
返信