IMX8M Nano :- eMMC Booting failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M Nano :- eMMC Booting failed

2,025件の閲覧回数
milav_soni
Contributor III

 

Hello,

We have build a custom Board which have "MIMX8MN1CVTIZAA" MPU.

We have successfully download L5.4.47-2.2.0_images_MX8MNEVK image in to eMMc via usb mode.

We use following cmd in win 10.

 

E:\camera_board_firm\image\L5.4.47-2.2.0_images_MX8MNEVK>uuu.exe uuu.auto-imx8mnddr4evk

 

Then we change boot mode in to eMMC and power on the board.

and boot log stuck on

[    2.236560] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator

 Please find attachment for whole emmc log.

please help me out.

Thank you 

0 件の賞賛
返信
1 返信

1,929件の閲覧回数
milav_soni
Contributor III

can anyone please help me out in this error?

 

0 件の賞賛
返信