I2C_LDD Component compiles without errors, silence on SDA, SCL pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I2C_LDD Component compiles without errors, silence on SDA, SCL pins

跳至解决方案
4,299 次查看
yusifnurizade
Contributor III

Hello,

 

I posted this question as open for the whole community (No activity on probes after successfully configuring and running I2C_LDD component) but it's been over two weeks so I am hoping this is a more appropriate place to post.

 

A brief summary; I am using Codewarrior 10.5 with Processor Expert. I've configured the I2C_LDD component and copied in sample code I found in Help On Component. I get no errors or warnings but when I go to run the code, the SDA and SCL pins are silent. I tried a fix I found on MCU on Eclipse (KL25Z and I2C: Missing Repeated Start Condition | MCU on Eclipse). I tried reducing the sample code as far down as just the I2C_Init function so I could just see the SCL pin running the clock. I contacted the manufacturer of the IC I am trying to communicate with and corrected my code as per their suggestion. All roads seem to point to the component configuration.

 

I've attached a copy of my initial attempt with the sample code. Later versions stripped out parts like the Term and Util and well as pieces of the code using I2C_LDD all the way down to just leaving the I2C_Init function. I put in the send string functions as a trouble shooting tool and I cannot see any besides the first one so whatever problem I am running into hits by the Init function call. Once I am communicating with the IC, I can reconnect with the manufacturer support but for now I could really use some advice on what's causing the silence.

 

Hope to hear from you,

Yusif Nurizade

Original Attachment has been moved to: I2C_Communication_Attempt_1_8b_2014.zip

标签 (1)
0 项奖励
回复
1 解答
3,940 次查看
yusifnurizade
Contributor III

All,

I've managed to resolve the issue I've been having and am posting the fix in case any one has a similar problem.

Originally, as seen in my wiring diagram, I wired the IC power and ground to the corresponding pins on the MCU. The digital logic analyzer showed the SDA and SCL pins as high so I did not think that the problem could be here. On a whim, however, I rewired on a powered prototyping board with a much higher current rating. As soon as I did this, I was able to see activity on both pins.

Thanks again for the help,

Yusif Nurizade

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,941 次查看
yusifnurizade
Contributor III

All,

I've managed to resolve the issue I've been having and am posting the fix in case any one has a similar problem.

Originally, as seen in my wiring diagram, I wired the IC power and ground to the corresponding pins on the MCU. The digital logic analyzer showed the SDA and SCL pins as high so I did not think that the problem could be here. On a whim, however, I rewired on a powered prototyping board with a much higher current rating. As soon as I did this, I was able to see activity on both pins.

Thanks again for the help,

Yusif Nurizade

0 项奖励
回复
3,940 次查看
Petr_H
NXP Employee
NXP Employee

Hi,

At first, please check that you have connected 4k7 pull-up resistor connected to I2C lines. The pins SDA, SCL should be "high" when no data are transferred from master.

Please check the error code that is returned by MasterSend/ReceiveBlock(). If the lines would not be in correct "IDLE" state, these methods would return ERR_BUSY.

To catch potential errors during communication, please enable the OnError event (in Events tab of the component inspector) and put some code there. To get detailed error information, use the GetError method.

Note: To enable these methods and events, you may need (If you already haven't do so) switch to Advance or Expert view mode (button at top-right in inspector view).

Please also note that the slave device has to be connected to the I2C pins, otherwise the communication always ends with an error, because the slave must send acknowledge after it receives the address etc..

Best regards

Petr Hradsky

Processor Expert Support Team

0 项奖励
回复
3,939 次查看
yusifnurizade
Contributor III

Petr,

Thank you for your reply. I apologize for the late response but I wanted to make sure I tried everything before coming back to the forum.

With regard to your suggestions, the pull up resistors are in place (the pins show high as default), I've added the OnError event and am checking the error code in the Send/Receive blocks. When I run the code, I get back a single 0 which I believe corresponds to the Send block and ERR_OK. Even if the receive block is not going through, however, I am curious why I wouldn't see some activity on the I2C pins. I've tried both digital logic analyzer and oscilloscope probes thinking I may have set an insufficient thresh hold but the channels just stay high with no changes.

I've spoken to the slave device's manufacturer and they confirmed the code and wiring setup should be producing some communication on the line. After checking and double checking I must admit, I am a bit stumped and am hoping for some advice. To that end, I am attaching my code and a schematic of my wiring connections.

Hope to hear from you,
Yusif Nurizade

0 项奖励
回复