How to set permanent ethernet mac address via fuse on iMX6 ULL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set permanent ethernet mac address via fuse on iMX6 ULL?

ソリューションへジャンプ
4,513件の閲覧回数
stefano_cappa_k
Contributor III

Hello everyone,

I have a custom board based on iMX 6ULL evk.

I'm using Yocto Sumo 2.5.1, with kernel linux-imx 4.9.88 and u-boot-imx 2017.03.

My board is working and I'm able to use the ethernet port without problems, but at every reboot the mac address is changing. Obviously, I'm also able to force this mac address via systemd-networkd and it's ok.

However, now I want to set a permanent fixed mac address into my board. So, at every reboot, the mac address will be always the same and my os will use it without to forcing it via systemd-networkd.

I need this fixed mac address while booting to be sure that every services in my os will use it while starting.

How can I do that for iMX6ULL?

Thank you.

1 解決策
3,951件の閲覧回数
stefano_cappa_k
Contributor III

I fixed this problem using fuses. However the command to run in uboot changes based on the board.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,952件の閲覧回数
stefano_cappa_k
Contributor III

I fixed this problem using fuses. However the command to run in uboot changes based on the board.

0 件の賞賛
返信
3,951件の閲覧回数
sekhavs275
Contributor I

ut Mac address is changing after every reboot. My board is working and I'm able to use the ethernet port without problems, but Mac address is changing after every reboot. Help me!

You can resolve your Lenovo laptop error code 0xc00000e9 by visiting us.

0 件の賞賛
返信