How to set permanent ethernet mac address via fuse on iMX6 ULL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to set permanent ethernet mac address via fuse on iMX6 ULL?

跳至解决方案
4,508 次查看
stefano_cappa_k
Contributor III

Hello everyone,

I have a custom board based on iMX 6ULL evk.

I'm using Yocto Sumo 2.5.1, with kernel linux-imx 4.9.88 and u-boot-imx 2017.03.

My board is working and I'm able to use the ethernet port without problems, but at every reboot the mac address is changing. Obviously, I'm also able to force this mac address via systemd-networkd and it's ok.

However, now I want to set a permanent fixed mac address into my board. So, at every reboot, the mac address will be always the same and my os will use it without to forcing it via systemd-networkd.

I need this fixed mac address while booting to be sure that every services in my os will use it while starting.

How can I do that for iMX6ULL?

Thank you.

1 解答
3,946 次查看
stefano_cappa_k
Contributor III

I fixed this problem using fuses. However the command to run in uboot changes based on the board.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,947 次查看
stefano_cappa_k
Contributor III

I fixed this problem using fuses. However the command to run in uboot changes based on the board.

0 项奖励
回复
3,946 次查看
sekhavs275
Contributor I

ut Mac address is changing after every reboot. My board is working and I'm able to use the ethernet port without problems, but Mac address is changing after every reboot. Help me!

You can resolve your Lenovo laptop error code 0xc00000e9 by visiting us.

0 项奖励
回复