How to select external Oscillator using processor expert in S32DS project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to select external Oscillator using processor expert in S32DS project

3,032件の閲覧回数
kashifsagheer
Contributor II

I am new on the processor expert and NXP 32bit MCUs. I want to select only the external oscillator in the clock setting.

pastedImage_1.png

pastedImage_2.png

  • How can I configure the external oscillator and then PLL
  • system clock should also be based on SOSC
  • Bus clock is also drive from SOSC

How can I verify#@ whether I select correct clock or not?

ラベル(1)
2 返答(返信)

2,892件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello kashifsagheer‌,

To enable/disable the clocks there's a little checkbox in the Clock Sources table:

pastedImage_1.png

In the Interface Clocks table you can select the clock source if you click in the SCS_CLK option:

pastedImage_3.png

If you change the SCS_CLK the BUS_CLK will have the same clock source.

Also in the Clock configuration table, if you click in the tab, more configuration options will be displayed:

pastedImage_4.png

Let me know if this helps you.

Best Regards,

Alexis Andalon

2,892件の閲覧回数
kashifsagheer
Contributor II

Hello Alexis,

Thank you!

0 件の賞賛
返信