How to know the irq number for the UART3 module on i.MX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to know the irq number for the UART3 module on i.MX6Q

跳至解决方案
2,487 次查看
yinliangren
Contributor II

   I'd like to set IRQ to CPU1 on i.MX6Q sabresd board like : 

                                   echo 2 > /proc/irq/irqnumber/smp_affinity

 But I didn't find the irq number for UART3 module, could somebody help me? 

BTW, the BSP version is 5.10.72_2.2.0.

0 项奖励
回复
1 解答
2,420 次查看
yinliangren
Contributor II

I've got the number, it's not a constant number. The irq number showed up after I ran an application to open and use UART3. 

在原帖中查看解决方案

3 回复数
2,471 次查看
Yuri
NXP Employee
NXP Employee

@yinliangren 
Hello,

   According to Table 3-1 (Arm Cortex A9 domain interrupt summary) of i.MX 6Dual/6Quad Reference Manual (Rev. 6, 05/2020) IRQ = 60 for  UART3 interrupt request.

Regards,
Yuri.

0 项奖励
回复
2,463 次查看
yinliangren
Contributor II

Hi Yuri,

   Thanks for your answer, but I haven't found the number 60 in /proc/irq/ as below:

root@imx6qsabresd:~# uname -a
Linux imx6qsabresd 5.10.72-lts-5.10.y+ga68e31b63f86 #1 SMP PREEMPT Tue Nov 23 06:02:20 UTC 2021 armv7l armv7l armv7l GNU/Linux
root@imx6qsabresd:~#
root@imx6qsabresd:~# ls /proc/irq/
100/ 291/ 72/
118/ 30/ 73/
123/ 31/ 74/
125/ 315/ 77/
147/ 32/ 78/
16/ 33/ 79/
17/ 34/ 80/
171/ 35/ 81/
178/ 51/ 82/
18/ 52/ 83/
181/ 57/ 84/
184/ 58/ 85/
19/ 62/ 86/
20/ 63/ 87/
21/ 64/ 88/
22/ 65/ 89/
221/ 66/ 90/
23/ 67/ 95/
24/ 68/ 96/
25/ 69/ default_smp_affinity
26/ 70/
28/ 71/

Could you tell me how to show 60 in /proc/irq/ ? Thanks a lot.

标记 (1)
0 项奖励
回复
2,421 次查看
yinliangren
Contributor II

I've got the number, it's not a constant number. The irq number showed up after I ran an application to open and use UART3.