How to Save ProcessorExpert Project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Save ProcessorExpert Project?

ソリューションへジャンプ
2,931件の閲覧回数
Vagni
Contributor IV

Starting working with CW 10.1 I realize a "Save Project" menu command does not exist.

It seems "Close Project" be the only way to save a project.

My question is due to the fact that yesterday CW crashed while I was setting an embedded component in a ProcessorExpert project: I lost all of my changes I made in one hour of work.

CW 10.1 asks me only when I close the CW project if I want to save the changes in the ProcessorExpert.pe file.

Is there any way to save the current project in CW 10.1 (both CodeWarrior and ProcessorExpert projects) without closing and then re-opening it?

0 件の賞賛
返信
1 解決策
2,771件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

Yes, there is a way (beside closing the project):

if the settings are not saved, then the component inspector (e.g. if you are on the CPU component) shows a star (*) if things are not saved yet:

Have the tab selected (so it has the focus) and press CTRL-S (for save): this should save all your settings.

 

BK

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,772件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

Yes, there is a way (beside closing the project):

if the settings are not saved, then the component inspector (e.g. if you are on the CPU component) shows a star (*) if things are not saved yet:

Have the tab selected (so it has the focus) and press CTRL-S (for save): this should save all your settings.

 

BK

0 件の賞賛
返信