How do you set up Serial_LDD (UART) in Processor Expert?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do you set up Serial_LDD (UART) in Processor Expert?

3,479件の閲覧回数
paulsawyer
Contributor I

With CW 10.5, and MK22DN512VLK5, Serial_LDD, selecting UART0,1 or 3 always shows an error than it cannot use *UART2* pins instead of the correct multiplexed UART pins.  It also won't build in this condition.  I may have to select UART2, generate the code and then fix everything so that UART3 is selected.  Has anyone else had this problem?

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

3,063件の閲覧回数
Monica
Senior Contributor III

Hello Paul,

was this suggestion helpful?

Please keep us posted :smileywink:

Best,

Monica.

0 件の賞賛
返信

3,063件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

I was able to select pins on all UART devices. Details for UART3 are attached. I have just verified it in CW V10.5.

Please note that the selected device must aleays match with corresponding pins otherwise PEx reports an error. In case you switch device, pins are not changed automatically in case there is possible to select more pins.

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信