How could I program S32k118EVB through OpenSDA?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How could I program S32k118EVB through OpenSDA?

1,648 次查看
andreialexandr1
Contributor I

Hi!

       I just bought a S32k118 EVB development board. I wrote a little code and tried to load it on the board, but unfortunately I can't start it. I think it's a problem with the board because after I connect it to the USB port, it doesn't show me anything (no LED is ON and debugger shows me this message: "PEmicro GDB Launch Failure : Unable to auto-detect debug hardware"), I also tried to change some hardware jumpers, but the problem remained.

      Does anyone know if there is a hardware problem, or I missed something?

Thank you!

0 项奖励
回复
1 回复

1,597 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Andrei Alexandru Dughila,

Sorry for late reply!
I just saw this question. Please post in the corresponding place for the next question. Only then can engineers in this field help you.
For this question, you can post it in S32K or S32 Design Studio.

Please check the setting of J107. According to the S32K118EVB-QSG, the S32K118 powered by 12V power source by default. If you want to debug it by USB port, then you should connect Pin2-3 of J107.

J107 S32K118EVB-QSG.png

Please learn this board by click Get Started with the S32K118EVB.

 

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复