HelPorting app from DPDK on x86 to NXP 2160

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HelPorting app from DPDK on x86 to NXP 2160

ソリューションへジャンプ
2,589件の閲覧回数
SysManOne
Contributor II

Hello!

 

Sorry for possible dups, I'm not sure for right place for the question also.

 

I develop an application uses DPDK on Intel x86 platform. Move it to NXP 2160 build binaries and try to run.

20-09-2022 13:52:43.576 10330 [TT2CP\main\425] %TTR2CP-I: Beging EAL initialization, be patient ...
EAL: Detected CPU lcores: 16
EAL: Detected NUMA nodes: 1
EAL: Detected shared linkage of DPDK
EAL: Multi-process socket /var/run/dpdk/rte/mp_socket
EAL: Selected IOVA mode 'VA'
EAL: VFIO support initialized
TELEMETRY: No legacy callbacks, legacy socket not created
20-09-2022 13:52:43.815 10330 [TT2CP\main\429] %TTR2CP-I: EAL is initialized
20-09-2022 13:52:43.816 10330 [TT2CP\main\438] %TTR2CP-I: Cleanup EAL ...
20-09-2022 13:52:43.889 10330 [TT2CP\main\442] %TTR2CP-I: Exit with exit_flag=0, rc=0

 

So, what i'm need to check additionaly ?

Thanks!

 

 

VAX/VMS forever
0 件の賞賛
返信
1 解決策
2,582件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Did you run LSDK 21.08 on LX2160A platform?

If yes, please do the app porting based on DPDK source code from LSDK 21.08.

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/dpdk.git

$ cd dpdk

$ git checkout -b LSDK-21.08 LSDK-21.08

 

元の投稿で解決策を見る

2 返答(返信)
2,578件の閲覧回数
SysManOne
Contributor II

In additions:

root@localhost:~/dpdk-extras/dpaa2# ./dynamic_dpl.sh dpmac.10 dpmac.9 dpmac.8 dpmac.7
Using board type as 2160
Using High Performance Buffers
mkdir: cannot create directory ‘/mnt/hugepages’: File exists

##################### Container dprc.2 is created ####################

Container dprc.2 have following resources :=>

* 16 DPBP
* 8 DPCON
* 8 DPSECI
* 4 DPNI
* 24 DPIO
* 2 DPCI


######################### Configured Interfaces #########################

Interface Name Endpoint Mac Address
============== ======== ==================
dpni.1 dpmac.10 00:00:00:00:0:10
dpni.2 dpmac.9 00:00:00:00:0:9
dpni.3 dpmac.8 00:00:00:00:0:8
dpni.4 dpmac.7 00:00:00:00:0:7

root@localhost:~/dpdk-extras/dpaa2#

 


root@localhost:~/dpdk-extras/dpaa2# export DPRC=dprc.2

VAX/VMS forever
0 件の賞賛
返信
2,583件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Did you run LSDK 21.08 on LX2160A platform?

If yes, please do the app porting based on DPDK source code from LSDK 21.08.

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/dpdk.git

$ cd dpdk

$ git checkout -b LSDK-21.08 LSDK-21.08