HCS12X and HCS08 cpu beans - Method DELAY100US - Has a undesired side effect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS12X and HCS08 cpu beans - Method DELAY100US - Has a undesired side effect

3,404件の閲覧回数
AndersJ
Contributor IV

The delay function not only delays, but it also writes to the COP preventing it from timing out.
This happens in PE beans of the CW 4.7 and CW6.2 era.

This is a undesired side effect to a delay, and should be removed.

PE team,
please explain why the delay was programmed like this.

0 件の賞賛
返信
4 返答(返信)

3,326件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

I'm sorry, but the original Processor Expert beans are no longer supported. If you need any change to the method, you can copy it into your own module and modify it or you can disable the code generation for the particular file and modify it there. 

best regards

Petr Hradsky

Config Tools Team 

0 件の賞賛
返信

3,319件の閲覧回数
AndersJ
Contributor IV

Assuming i would purchase ”these products” today,
for HCS08 AND HCS12X,
which CW and PE versions would that be?

What additional improvements and features will I get today
compared to my currently used V6.3 and V4.7.

0 件の賞賛
返信

3,391件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Is this also happening on codewarrior 11?

Regards

 

0 件の賞賛
返信

3,386件の閲覧回数
AndersJ
Contributor IV

Cannot say, I do not use CW11.
Open a CW11 project, enable the method, and read the source code.

0 件の賞賛
返信