FreeCntr component can't Enable/Disable Events?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeCntr component can't Enable/Disable Events?

ソリューションへジャンプ
1,985件の閲覧回数
jgirard1
Contributor III

I am working with CodeWarrior 5.1 for S12(X).  My target is 9S12XA256.

I am adding the FreeCntr component and setting it up to be an output compare that interrupts at a specified rate.

There is no way to disable the interrupt event.  The Enable/Disable Event methods are grayed out in Processor Expert and nothing I do will enable them.  I tried connecting it to different timer sources, shared timers, individual PIT timers, etc.  Nothing works.  The Enable/Disable events are always grayed out.

How do I stop this FreeCntr componet from interrupting when I do not need it anymore?  Aside from going directly to the registers myself with my own code, I think there is something seriously wrong with this component and the way it was implemented.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,836件の閲覧回数
jgirard1
Contributor III

The events in the Events tab have to be enabled first before the Enable/Disable methods will be activated in the Methods tab.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,837件の閲覧回数
jgirard1
Contributor III

The events in the Events tab have to be enabled first before the Enable/Disable methods will be activated in the Methods tab.

0 件の賞賛
返信