FLASH_LDD issue with safe write and FTFE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLASH_LDD issue with safe write and FTFE

2,180件の閲覧回数
davidschroeder
Contributor II

I have a project that was running on a K20DX256 that stores some parameters in flash using the IntFLASH and FLASH_LDD components. The project is transitioning to a K20FX512 in order have more ram available when. When I did this I started to receive hard faults when writing to flash. The hard faults would always occur at the the same address, but I was able to complete several other flash writes successfully before getting the fault. To further complicated the issue, once I'd received the hard fault during the write subsequent reads of the same memory would also generate a hard fault.

Digging into it it looks like there is a bug in the IntFlashLdd2_CommandCompleteInterrupt function generated by FLASH_LDD. This code has logic to allow writes of less than the 8 bytes by reading the values that are currently in flash and merging it with the data to be written. However, if the data being written lines up such that it's only in part of the top 4 bytes then the data that is read back is not properly merged resulting in the hard fault. The code snipet below shows the fix that worked for me.

...

      FlashPrgUnitAddr = DeviceDataPrv->CurrentFlashAddress - DstAddrOffset;

      CurrentFlashPrgUnitData[0] = ((uint32_t *)FlashPrgUnitAddr)[0];

      CurrentFlashPrgUnitData[1] = ((uint32_t *)FlashPrgUnitAddr)[1];

      if(((DataToPrg[0] & DataToPrgMask[0]) & (~CurrentFlashPrgUnitData[0])) > 0U) {

        DeviceDataPrv->CurrentErrorFlags |= LDD_FLASH_MULTIPLE_WRITE_ERROR;

        return;

      }

      if(((DataToPrg[1] & DataToPrgMask[1]) & (~CurrentFlashPrgUnitData[1])) > 0U) {

        DeviceDataPrv->CurrentErrorFlags |= LDD_FLASH_MULTIPLE_WRITE_ERROR;

        return;

      }

      DataToPrg[0] = DataToPrg[0] ^ (~CurrentFlashPrgUnitData[0]);

      DataToPrg[1] = DataToPrg[1] ^ (~CurrentFlashPrgUnitData[1]);                           <<---- This line was missing!

      DeviceDataPrv->CurrentDataSize = PrgBytesCount;

      DeviceDataPrv->DataCounter -= PrgBytesCount;

      FTFE_PDD_WriteFCCOBFirstLongWordData(FTFE_BASE_PTR, DataToPrg[0]);

      FTFE_PDD_WriteFCCOBSecondLongWordData(FTFE_BASE_PTR, DataToPrg[1]);

...

0 件の賞賛
返信
3 返答(返信)

1,763件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

thanks for reporting this issue. Do you need the hot-fix for it or it is sufficient for you to disable code generattion of this component and fix it manualy?

Anyway the fix will be published within CW V10.6 in Q1/2014 - Q2/2014

Please let us know your decission. We are sorry for inconvenience.

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信

1,763件の閲覧回数
davidschroeder
Contributor II

Vojtech,

      I can get by with disabling code generation and manually fixing the problem for the time being.


Thanks,

   ~Dave

0 件の賞賛
返信

1,763件の閲覧回数
vfilip
NXP Employee
NXP Employee

Thanks

0 件の賞賛
返信