Error in component bean eeprom in 9s12g128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in component bean eeprom in 9s12g128

2,176 Views
rpolanias
Contributor I

Hello everyone,

I have a project with codewarrior 5.2, Processor Expert and MCU 9S12G128.

when adding the EEPROM bean I have this error:

+IEE1
+ERROR: Compiler option -CpPPAGE=0x15 (address of PPAGE register) or -CpPPAGE=RUNTIME must be set to compile the generated code correctly (current target settings, Compiler for HC12, Options, Code Generation tab, PPAGE register is used for paging). After compiler option change, run Code design to apply the change in Processor Expert. For details, see Help of the component.

+IEE1
+ERROR: There are errors in component, it is impossible to generate code

I appreciate any help. 

 

Labels (1)
0 Kudos
Reply
3 Replies

2,028 Views
elizabethbrown2
Contributor I

hello,

Do you find exact reason behind this error?

and I think there is a way to generate code. Will be back soon.

Thankyou.

0 Kudos
Reply

2,028 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Eliza and Ricardo,

The solution for your issue can be found in the community link below:

I use PE for EEPROM. 

I believe it helps.

Best Regards,

Diana

0 Kudos
Reply

2,028 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Ricardo,

Could you please share your whole project?

After that, I can try to check the root cause of your issue.

Thank you.

Best Regards,

Diana

0 Kudos
Reply