Error in component bean eeprom in 9s12g128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in component bean eeprom in 9s12g128

2,282件の閲覧回数
rpolanias
Contributor I

Hello everyone,

I have a project with codewarrior 5.2, Processor Expert and MCU 9S12G128.

when adding the EEPROM bean I have this error:

+IEE1
+ERROR: Compiler option -CpPPAGE=0x15 (address of PPAGE register) or -CpPPAGE=RUNTIME must be set to compile the generated code correctly (current target settings, Compiler for HC12, Options, Code Generation tab, PPAGE register is used for paging). After compiler option change, run Code design to apply the change in Processor Expert. For details, see Help of the component.

+IEE1
+ERROR: There are errors in component, it is impossible to generate code

I appreciate any help. 

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,134件の閲覧回数
elizabethbrown2
Contributor I

hello,

Do you find exact reason behind this error?

and I think there is a way to generate code. Will be back soon.

Thankyou.

0 件の賞賛
返信

2,134件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Eliza and Ricardo,

The solution for your issue can be found in the community link below:

I use PE for EEPROM. 

I believe it helps.

Best Regards,

Diana

0 件の賞賛
返信

2,134件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Ricardo,

Could you please share your whole project?

After that, I can try to check the root cause of your issue.

Thank you.

Best Regards,

Diana

0 件の賞賛
返信