Error exporting to Keil uVision

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error exporting to Keil uVision

ソリューションへジャンプ
2,114件の閲覧回数
johncameron
Contributor I

Hello,

I have a question regarding uVision project export from Driver Suite 10.4.2

Micro: PKEAZ128 64 pin.

Keil MDK:

Version 5.12.0.0

Pack: http://www.keil.com/pack/Keil.Kinetis_KEAxx_DFP.1.1.0.pack

Driver Suite 10.4.2

Selected device: SKEAZ128MLH4

I can generate the code in Driver Suite.

To export to uVision I am trying the following;

File->Export

Inline images 1

Inline images 2

Inline images 3

Inline images 4

But on clicking finish I get this;

Inline images 5

What is my mistake?

Thanks,

John

0 件の賞賛
返信
1 解決策
1,936件の閲覧回数
johncameron
Contributor I

Thanks Marek,

I have tried a couple of versions of these instructions, none match my installation exactly.

However, I have fixed it.

I had 2 versions of Keil's MDK and 2 version of Processor Expert. So I uninstalled all of them and reinstalled only the latest with the packs I needed.

John.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,936件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi John,

I am sorry but I cannot see screenshots that you have posted (an error on the page). But I know that there were error in the Keil MDK 5 for SKEAZ family (an error was reported when the exported project was opened by uVision). There is available Freescale Processor Expert Add-On for MDK 5.12 installer that fix the problem, see page Freescale Processor Expert Add-On for MDK 5.12

Detailed instructions (how to install, setup and configure the export ) are available on the web page Using Keil μVision 5 with Processor Expert | MCU on Eclipse.

Best Regards,

Marek Neuzil

0 件の賞賛
返信
1,937件の閲覧回数
johncameron
Contributor I

Thanks Marek,

I have tried a couple of versions of these instructions, none match my installation exactly.

However, I have fixed it.

I had 2 versions of Keil's MDK and 2 version of Processor Expert. So I uninstalled all of them and reinstalled only the latest with the packs I needed.

John.

0 件の賞賛
返信