Eclipse-based plug-in on Mac OS X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eclipse-based plug-in on Mac OS X

4,098 Views
cardoso
Contributor II

Anyone get this working on Mac OS X?

I follow the installation instructions but after the installation, it raise an error message:

An internal error occurred during: “Open last Processor Expert project”.

java.lang.NullPointerException

And in the log file:

!ENTRY com.freescale.processorexpert.core 4 0 2013-09-07 01:45:19.428
!MESSAGE reg.getExtensionPoint is empty

!ENTRY com.freescale.processorexpert.core 4 0 2013-09-07 01:45:19.531
!MESSAGE No com.freescale.processorexpert.core.PEservice extension found!

!ENTRY com.processorexpert.core.ide.wizard.ui 2 0 2013-09-07 01:45:29.810
!MESSAGE External elements location /Applications/eclipse/ProcessorExpert/Config/PE/CPE/wizard_data/wizards/components does not exist

Thanks

6 Replies

3,520 Views
maxpiepenbrink
Contributor II

I was able to set up Processor Expert ("Driver Suite") in OSX with just stock Eclipse Kepler. It takes some extra setup time but it works.

3,520 Views
krekeltronics
Contributor II

Any progress on this? I have a pretty nice Kepler installation going to stay in OS X. It will be cool to see if Processor Expert might be usable as well!

Cheers,

Patrick

0 Kudos
Reply

3,520 Views
liborukropec
NXP Employee
NXP Employee

Hello,

Driver Suite 10.5 will support MAC OS; it should be available by the end of this year. The upcoming Driver Suite 10.4.1 Update will have better support for MAC OS even it is not officially supported yet.

Best regards,

Libor Ukropec

Processor Expert Team

0 Kudos
Reply

3,520 Views
vfilip
NXP Employee
NXP Employee

Hello,

this is currently not supported and as far as I know that there is no plan to support PEx plugins for MAC in near future. However I have passed this request to our management.

Best regards

Vojtech Filip

Processor Expert Support Team

3,520 Views
ghemstreet
Contributor II

Which Processor Expert product are you trying to install? QCS, Driver Suite or Component Development Environment?


0 Kudos
Reply

3,520 Views
cardoso
Contributor II

I'm trying to install the Driver Suite 10.2

0 Kudos
Reply